Hi. !
input =5V, Vout=1.2V, Ioutmin=300mA, Ioutmax=2A, controller TPS57112q1, allowed output voltage fluctuation 5%, used capacitors: ceramic e.g. output capacitor 44uF/5mohm, selected switching frequency 1666kHz (to save the size of L and Cout)
compensation Network type II: take power stage as a voltage driven current source and forget the double LC-pole. you have just a pole created by Cout and Rload (Vout/Ioutmax) and a zero created by Cout and ESR of output capacitor. Gmps, gmea mentioned on the data sheet are enough to design a compensation network of type two.
pole is at 1.95kHz and Zero at 866kHz.
I have taken crossover frequency recommended by T I (66kHz) refer the page 20,
-I put just a zero with pole of plant together and pole of network with zero of plant.
But load regulation (change of load current from 300mA to 2A ) is very bad: output voltage goes down to 1V (more than 20% ).
Now I have to accelerate the controller: I could shift cross over frequency to e.g 300kHz.
it looks better but not enough.
I have to use compensation network type III.
Questions 1: why I have to change the model of the plant from single pole and zero (explained above ) to double complex pole generated by LC for type III compensation?
Question 2: DC gain of simple model is Gmps*Rload why I have to use Dc gain of complex type to Vin/Vramp (not more Gmps*RLoad) ?
Question 3: I could not find the Vramp on the data sheet of TPS57112q1 for example it is mentioned clearly on the data sheet of TPS40195 (Vramp =1V)
I hope many can help me.
regards
Bishnu