I have used the TPS40170 in a design. I have made some prototypes and due to an overlay error, a cap and resistor were swapped. The end result was that the EN pin on the TPS40170 was left floating on some of my prototypes. Now that I have swapped the resistor and cap, some start up, and some don't. Some start up and cannot be disabled with the EN pin. The datasheet says the EN pin must not be left floating. If it is, can damage to the IC occur so that the enable pin no longer works correctly, or at all? The power supply design is all OK and has been tested on earlier prototypes, this error was introduced on the latest round of prototypes.