Other Parts Discussed in Thread: TPS61500
Hello,
First, my apologies if I'm not writing in the right forum but I'm a bit lost with this issue.
I'm trying to design a lamp for a vision machine application. It consists on 9 ultra bright leds. The connection of these leds will be in serial so I need a constant current through them.
Each led consumes 20 mA and 3.3V and the total power I need will be around 0.6W. Furthermore I also want to strobe them with peaks of 100 mA, I'm thinking in a strobe mode not only continuous.
At this point I dont know if a constant current regulator could fit in this application or there is a led driver with a built-in function that helps me to implements the strobe mode. Any suggestions... guidelines... ??
Thanks in advance.