Customer has following question
I am using the LM3406HV in a design, and my issues are as follows.
1) Ron resistor is 500K
2) MSS1278-104 is the inductor part number (100uH)
3) Cout is 10uf
4) All other values are straight out of the data sheet.
Everything seems to run fine and unit functions straight as the math predicts until we use the PWM dimming function. Once we begin to dim (17.7K dim freq) we run all the way down to 1% and when we return back to 100% the output switching frequency drops by 1/2, and it will overshoot its current until it bounces off the 2A hard limit then the whole IC resets, and returns back to the correct switching frequency, and correct current target.
Also, after the unit is dimmed, and output frequency is stuck at 1/2 the target, I can reset the part by grounding the Ron pin and the the unit will fix itself, and return back to the target frequency.
So long story short... I cant dim this unit. When I do, it latches into the lower switching frequency, and wont regulate to its current target until it is rest.
Can you help.
**** end customer question
Regards,
John Wiemeyer