This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum current capability of

Other Parts Discussed in Thread: LM5118, LM5160

Hello 

Need a dc-dc nonisolated converter 

input 6v to 50v

output 12v

output current 5A

Using w-bench  with refrence to earlier post  i had started my first design with LM5160 , but failed , then suggested part is LM5118 

Now W-bench is showing ouput for 5A but  in datasheet current at 12 v for buck boost design is 3A and overcurrent limit at 4.5 A .

Please provide  solution to this problem and suggest any other component if LM5118 is not suitable .