This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54295 Power dissipation and Input current information needed

Other Parts Discussed in Thread: TPS54295, TPS54260

Hi,

Customer of mine is designing their power stage using dual channel DCDC – TPS54295 and TPS54260. Please see the attached diagram for details.

I’ve few questions:

- Could you advise the Pd, temperature, input current on the dual channel DCDC (TPS54295) circuit. I’ve tried to simulate TPS54295 using SwitcherPro but only limited information available in the SwitcherPro.

- Referring to the pg2 in the attachment, could you advise why the converter showing the max temp of 35 only? Does it mean this converter dissipate power of 764mW @ 35 degree?

I’ve also attached the schematic for both TPS54260 and TPS54295 for your reference.

Thanks

 6215.Power_Stage.pdf