I could use some help with the bq34Z100 integration. I have an EV2300 EVM Interface board and a bq34z100EVM board. The battery I am using is 855085-2S 7.4V 4000mAh Lithium Polymer pack that was created for us. The fuel gauge (in our case) is not inside the battery pack, but rather on our digital board. I modified the bq34z100EVM board to match my design of the fuel gauge on the board. I followed the instructions to program the parameters into the data flash and calibrate it. I believe that I chose the correct board type when starting the bqEVSW software. I followed the instructions in “Identifying unknown chemistry simple discharge test – 24 hrs”. I now have a text file with the data. I downloaded a trial version of MathCad 15 software, but am having problems understanding how to use the chemselect.cont.mcd spread sheet. I also have questions on how to generate the golden flash image and the best way to load it my digital board. Can you assist?