Sir,
I want to develop a AC-DC converter with
1) I/P volt.= 220V +/- 10%
Output= 105Vdc/0.7A
2) I/P volt.= 220V +/- 10%
Output= 245Vdc/1.5A.
output ripple voltage = 0.02%
All outputs must be isolated from each other.
So for this configuration Which topology should i have to go ( Flyback or forward). And please suggest me any suitable IC. This power supply is industrial grade rugged.
I already work with flyback converter with uc 3844,3845 and other PWM ics like power integration, fairchild, ST, Onsemi. Now this application is critical in term of ambient temparature ,O/P ripple , load regulation so need your help.
Thanks & regards
mahesh