This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiphase converter using UCD9224 and UCD74111

Other Parts Discussed in Thread: UCD74111, UCD9224

Hi ,

Kindly review the design and configuration file for our 4 phase 1V supply using UCD9224 and UCD74111.

The specs for the design are:

1. 12V to 1V @ 48 A (SoC requires only 40A)

2. 4 phases at switching frequency of 700KHz

3. No phase shedding at low loads

4. Current sensed using 2mOhm sense resistor

5. 1V Enabled using the the seq1 pin (Active High)

Schematic:[

Configuration:

Also, Please share with me any documents about layout guidelines for the power driver UCD74111. 

Thanks

Ashok