hi,
As I use the tps40077 in my system, it's for the dc-dc 24v-15v. As I test this circuit in the constant load(4A), it works fine, but my real load is the 1khz pwm output, Irms=1.5A.
As the pwm output stage, there will be inductor buzz noise, and the 1khz frequency is in the range of our ear. it looks like the response speed of the tps40077 is not so fast.
Is there any one have this kind exprience to reduce the inductor buzz noise? Thanks a lot!