This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DV2002 or BQ2002 Value of RB1 and RB2 for one or two cell battery

Other Parts Discussed in Thread: BQ2002

Hi,

I want to charge one or two cells with BQ2002.
At the schematic of DV2002 is the value of RBn shown for 4 and more cells.

Will I be right with the assumption that one cell is directly connected to BAT ?
With two cells a divider is needed like 330K to 330K ?

Thanks for your help.

Claus