This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Solar charging of Lithium cell without exceeding MSP430 VCC limit

Other Parts Discussed in Thread: BQ24210

Hi,

I have an application where I need to use a solar cell to charge a Lithium battery that powers an MSP430. I looked at the bq24210, but it allows the battery voltage to go up to 4v, which would destroy the MSP430 that is being operated. Is there a way to do this cleanly, or do I need to have a switcher downstream of the battery to make sure I stay below 3.6v while the battery is being charged.

Lloyd

  • I think you definitely need to use a DC-DC converter to lower the Li-ion voltage to 3.3V or lower. The voltage of a Li-ion battery is well beyond MSP430's maximum ratings. You can use TI's Power Architect to select an appropriate chip and circuit to do the job.