This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

If TPS23754 can power up to 33W??

Other Parts Discussed in Thread: TPS23754, TPS23754EVM-383

Dear Sir

Good days,

May we check if TPS23754 can power up to 33W(12V/2.75A)??due to spec show power up to 30W.

If yes, may we direct use TPS23754EVM-383 to driver, is any thing to change?

                                                  Best regards,

                                                                 Bogey

 

  • The TPS23754EVM-383 dc/dc converter (with input inserted to dc/dc primary) may be able to deliver 33W at the output in a laboratory type condition at room temperature. You could try a bench test to see where output foldback occurs with respect to dc input voltage. Long term operation over more conditions would require further evaluation.