For the LM2623 - DC/DC Boost Converter, I am doing some battery life calculations and would like to know the efficiency of this convertor with a load of 5 mA at the output voltages of 10, 12 and 14 VDC.
Because this will be a battery operated device the Vin will vary from around 3.2 volts down to 1.8 volts. (Input source = 2AA batteries in series)
I was only able to find one graph for efficiency on the LM2623 data sheet. That was “Efficiency vs. Vin at Vout = 5 volts”.