This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM for Peltier Thermoelectric Module

Does anyone have a suggestion for a PWM I could use for the following application.  I want to use a Peltier thermoelectric module (TM) to power a mini DC water pump.   The specifications for the TM power supply and water pump are posted below.  The heat source for the TC can fluctuate resulting in a change in output for the TC, which is why I've posted both the maximum range outputs and the normal operating range for the outputs.

Let me know if you have any suggestions for a PWM that could work in this application, or if you need additional information.

Cheers,

Ken

  Specification
  Peltier Power Supply DC Mini-Water Pump
  Maximum Range Normal Operating Range Maximum Range Preferred Operating Range
Open Circuit Output Voltage 2-10 6-8    
Matched Load Output Voltage 1-5 3.5-4.5 5-12  
Matched Load Power (W) 1-8 5-6 1-5 4-5
Matched Load Resistance (ohms) 2.6-3.2 3.0-3.2    
Matched Load Current (A) 0.4-1.6 1.0-1.3 0.1-0.4 0.3-0.4