Hi ,
We build 3kW Interleaved PFC works from 90-265V AC and it is Working Fine
.Now the requirement has come to Work form 120V Battery.
When I feed 120V DC to the input of the rectifier, it is Able to Boost to 400V. When we load 2.6kW in the Following Pattern the DC Bus Drops Drastically from 400V to 200V.
Is there any way we can make UCC28070 as Only Boost Converter with High Band Width (without PFC) so that The DC Bus Will not drastically.
Can anybody help me to find What are the Changes to Be done on UCC28070 Schematic to make Suitable for DC Input
Thanks in advance.