This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610

Hi

I have some questions would like to ask as following:

1.Does precharge and termination are includes in safty time?

2.If increase the resistance for rsense to 50m ohm, whether could increase accuracy?

Please refer ELECTRICAL CHARACTERISTICS as following:

current regulation –fast charge

Rsense=10m ohm

if fast charge =3A

Vsense=30mv  accuracy around +/-4%

fast charge =1A

Vsense=10mv  accuracy around +/-25%

 Change Rsense to 50m ohm

Vsense=50mv accuracy around +/-3%