This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq3060 gas gauge data flash



hello,

Can any body explain me that

the real meaning of LT/ST1/ST2/HT Chg Voltage, is this voltage is equal to the battery charge voltage.

or it is a different value from the battery charge voltage. How can i decide these values.

we are using LiFePo4 6.4 Volts, 9.6Ah battery with BMS.

Thanks and Regards

Santosh