Hi TI ,
I have a few queries on TPS65217.
1.In page 20 of TPS65217 data manual , it is said that LDO_PGOOD output goes high when LDO1 and/or LDO2 are enabled . This is creating a lot of confusion .
Is it and or or??
2. When the TPS65217 is in sleep mode only LDO1 will be on . In that case does LDO_PGOOD be high?
3. To wake it up from the sleep mode if we press the PWR button does the PMIC toggle the WAKE_UP signal and the processor in turn has to come and enable PMIC_PWR_EN signal to enter active state . Is my understanding correct ?
4.Can the device be powered off by pressing the power button of PMIC TPS65217 ? Looking at the datasheet i understand that feature is not possible.
Thanks in Advance.
Best Regards,
Rajesh N