This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6595x audio section

Hello,

In our application we need on board mic, speaker (not earpiece) and headset mic and headset speaker.

We are doing above by using interface available in TPS65951:

On board

Mic: MIC.MAIN.P,MIC.MAIN.M

Speaker: Predrive outputs for 8 ohm speaker with class D amplifier (mono)

Headset:

Mic: HSMIC.P, HSMIC.M

Speaker: HSOL,HSOR

We need headset speaker and headset mic detection in the above explained application. We are using GPIO2 as suggested in TRM for headset speaker detection but for mic detection we are planning to use GPIO1 for it.

Would it be possible to use GPIO1 for the headset mic detection? If yes, is it possible to switch between on board and headset by software?