This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Lead Acid Battery Charger for 12V, 7.2AH battery

Other Parts Discussed in Thread: BQ24703, BQ24702

Hi, Kindy suggest design with circuit diagram for above battery charger with input of 85V to 265VAC

Regards   Atul Bhakay

  • Hello Atul,

    One option would be to use the circuit diagram in the bq24702 and bq24703 multichemistry chargers datasheet.  They can charge your lead acid battery with an input from an AC Adapter.  The voltage input is limited to a maximum of 30 volts, so you should be able to use any adapter from any laptop which has a universal voltage input of 85-240VAC.  Otherwise, you can design your own adapter for that input voltage range.

    Thanks,