This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206 / Reccomended Operating

Guru 20090 points
Other Parts Discussed in Thread: TPS51206

Hello,

In the data sheet of TPS51206 , there are below description.
 
------------------
<Data sheet P.1>
VTT Termination Regulator DESCRIPTION
 – Output Voltage Range: 0.5 V to 0.9 V
 
<Data sheet P.2>
Output voltage Range :VTT, VTTREF, –0.1V ~ 3.5 V
------------------
Q1
Why there are two of the  output voltage range in the datasheet?
  Because of VTT and VTT REF can be off by S3/S5 pins ?
 
Q2
In the datasheet P.2, there is VDDQSNS input operating range as –0.3V ~ 3.6V.
So, I think VTT voltage will be configured -0.15V  ~1.8V
Is my understanding correct ?
 
 
I understand that  VDDQSNS voltage should be 1.2V ~ 1.8V for DDR2/DDR3/DDR3L/LPDDR3.
But please kindly let me know.
 
Best Regards,
Ryuji Asaka