Hello,
I designed uTCA shelf board with two TPS2359 power distribution controllers on it.
Looks strange, but I fail to communicate with them via i2c: no acnowledge from any of the two TPS2359 connected.
I've tried several hardwired addresses, than wrote an i2c bus scanner - nothing helped.
I use MSP430 i2c hardware programmed to 100kHz SCL clock rate. It works OK with other devices.
What could be a reason for TPS2359 i2c to not to reply/acknowledge?
I looked through all the pins: nothing suspicious.
Could a thermopad be a reason? There is no wording in the datasheet what to do with it. I left it isolated.
Unfortunately it is much more difficult for me to try connect it now (the pad is under soldered QFN36) than to ask for your help here.
Any comments / ideas?
Thank you.