Other Parts Discussed in Thread: TPS2226A, TPS2226, TPS2224, TPS2223
Hello,
we made a design with 1520 Dual PCMCIA Controller from TI. We are using TPS2226ADB for power switching. The design is made as PCI add-in card, so we are using only PCI parallel interrupts.
At least, this is not a very special or even complex design. That I was thinking before we started production of initial batch. Now, after a few days testing, we have failure rate of 25%. We found out, that the 2226ADB is burning away. This chip is showing the same burning areas more or less the same on all burned chips. This areas are corrosponding to both 12V input pins. BUT, there are no cards inserted into the cardbus slots. So no current should be used by this input pins.
We double checked schematics, every thing is ok, regarding datasheets and also reference design. So we went deeper and tried to check for the serial protocol between 1520 and TPS2226A, but we also found a note in the datasheet, that definition of D0 to D10 can be seen at control logic table, but this table is not part of the datasheet ...
Maye somebody has seen that before?
Thanks Jens