This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3808G01 / sequence of power supply for Vdd,Vsense

Guru 20090 points
Other Parts Discussed in Thread: TPS3808
Hello,
 
Are there any power supply sequence for VDD and Vsense ?
 
For example, Vsense power on(2.5V) ---> VDD power on(3.3V).
In this case, Vsense power is biased before VDD power up. (i.e. Vsense =2.5V, Vdd=0V)
 
I think that there is absolute voltage rating of Vsense as -0.3V ~ 7V.
So, there is not power supply sequence requirement for Vdd,Vsense.
 
Best Regards,
Ryuji Asaka