I would like to have the rise and fall transition rate specification clarified. This item is found in the recommended operating conditions section and is defined as a max of 100ns/V. Can you verify that this is means, in my own words, that the transition time from low to high must be faster than 100ns/V? What will the part do (or not do) if the transition time is slower than 100ns/V?