This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq51013b

Hi 

I want to use bq51013Bevm with bq500211Aevm.

I thought about buying them both, will they work together? does the firmware on the msp in the bq500211Aevm is on it or do I need to put it?

can I change the firware?

what is the max power those modules can transfer?

where I can find recommended coils for the bq51013Bevm? does it come with one? 

thanks in advanced,

  • Q1--I thought about buying them both, will they work together?

    A1—Yes, Qi certified units will work together.  Also both are WPC 1.1 certified and will feature Foreign Object Detection (FOD)

    Q2--does the firmware on the msp in the bq500211Aevm is on it or do I need to put it?

    A2—The 211A will program the MSP430 no additional programming or firmware is required by the user. See data sheet Page 16 for additional info.

    Q3--what is the max power those modules can transfer?

    A3—5W (5V at 1A).

    Q4--where I can find recommended coils for the bq51013Bevm? See does it come with one? 

    A4—See EVM User’s Guide Bill of Materials.  Also see FAQ in this forum.  Yes EVM comes with one.

  • thank you very much for fast and accurate answer.