This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unused UCD7242 output

Other Parts Discussed in Thread: UCD9222, UCD7242

Salutations,

I am capturing a schematic using the UCD9222 to control two output rails. I am using two phases of one UCD7242 for one rail since it exceeds 10A, however my second rail is less than 10A and only requires one phase of a second UCD7242. Can I leave the unused pins of the second phase not connected and expect it to operate as intended, or is there any special consideration when attempting this? Thank you.