This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Current limitation] LM2676-ADJ

Hello,

I want to fix a +12V potential in the output with a +24V input.

My problem: When the output current is higher than 600mA (with a charge of 20R), the voltage falls progressively.

All the capacitors are low  ESR, and dimensioned by the datasheet.

The shottky diode is a fast diode for switching power supply.

The inductance is for switching power supply too.

I had ask for an eval and I have comparativ mesure.

The eval have a LM2670-ADJ, so, the frequency is doubled.

Comparative mesure with the eval in signal 1 and my circuit in the second signal.

The load is  500 mA.

With this load, i have no problem, +12V without a lot of ripple in output.

Now with 1A Load:

With this charge, I have around 10V.

I hope someone has an idea to solve my problem?

Thank you for reading this,

Best regards,

Lucien Badoux