This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Searching for buck converter with the ability to limit Iout +/-5%

Hi,

is there a TI buck converter where the output current can be limited at a specific value?

Input voltage should be 16...35V, output voltage 13,6V (as long as the current limit is not reached). When the output current reaches the limit e.g. 1A (programmed by a shunt resistor for example) this max. current is held by reducing the output voltage. No foldback please.

The behavior should be similar to a L200 linear regulator. I know ST has a converter like this: L6902D

Thank you for your help!