Could somebody provide ESD rating values (human body model and contact discharge) for the TPS63000?
Best regards
Martin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could somebody provide ESD rating values (human body model and contact discharge) for the TPS63000?
Best regards
Martin
The TPS63000 meets standard 4kV human body model (HBM), 1.5kV charge device model (CDM), and TI does not specify machine model. If additional ESD protection is needed, refer to Texas Instruments' ESD protection devices http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?family=analog&familyId=1441&uiTemplateId=NODE_STRY_PGE_T for an economical solution.