been using a tps61202 for a sloar charger. tps61202 is included in the first module that converts the input from the solar panel (max of 6V) to 5V. its output will be then forwarded to the next module that charges a lithium ion battery.
i have used the schematic on page 1 of tps6120x datasheet (lower part). As I have observed, there were no much difference bet the one i used and the one shown in the evaluation kit. I know that it was not the same circuit that is shown in the evaluation kit but there were instances that the circuit worked. but now, its not functioning. should i change to what is shown on the eval kit?
or maybe you can recommend a more 'stable' buck boost converter for an input of at most 6V.
thanks.