We are manufacturing PSU in reasonably large qty and continuously have a "noise problem" where the synch FET gate drive is "spiked" by the rising edge of the voltage on its drain pin. This spike causes us the predictable grief in EMC and output rail "noise" let alone being a reliability issue.
We have tried numerous Qgd/Qgs ratio around 1.5 down to 1.1 and Qgate(tot) around 27nF-50nF - and still have a yield problem. Maybe the answer is to ensure this synch MOSFET ratio is always less than 1 ? or is TI able to state it should be less than 0.80 etc ..
It seems a possibility the manufcaturer - knowing the threshold gate drive capability should be able to specify the Qgate(total) and Qgd/Qgs ratio to ensure correct performance ??
Can anyone help with some experience in this issue ?
Rgds
DonW