This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Design of Power Switch between Main Power and Battery

Other Parts Discussed in Thread: UC27131

Hi ,

I am designing  one product with battery back up .The Li-Po battery charger (2 Cell ) Bq24103RHLR controlls the battery charging .

Once main power connects , then product (board) must powered and battery  should also charge . When main power disconnects , then board should drive from battery without any power fail .

The i/p power =12V , Bat voltage = 8.4V , Board current consumption =1A

I tried with simple P-MOSFET but  100ms delay exits between switching  so that board gets restarted .

Let me know any power switch /circuit for my requirment .

Thanks & Regards

sgp