Hello,
I am in the middle of designing a power circuit for an FPGA based system. I am using the PTH04000 and the PTH05050W to derive the voltages for the core and I/o respectively. I am also using a tracking LDO TPS74301 for deriving a quiet analog rail. I need all these three rails to rise following the same ramp rate. Hence, i have tied the auto track pins of both the PTH`s together and have given it to the TPS74301 track input through a resistor divider network calculated to yeild simultaneous sequencing.
Has anybody attempted this kind of thing before , are there any gotcha`s that i must look out for ?
Is there any way for me to estimate the ramp rate of the entire system ? I looked around but could not find any kind of models for the PTH`s.
Any help would be greatly appreciated .
Thanks!
Sornam