This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem about the TPS54317

Other Parts Discussed in Thread: TPS54317

Two chips of TPS54317 are used in my PCB board. But the output of the 54317 is 0V. There is no evidenct to show this chip is working. I don't why.

With the pull-up resistor, the PWRGD is always high whenever the ENA is asserted or not.

The PH, BOOT,VSENSE pins are 0V.

The VIN is 3.3V, I have comformed it for several times.

Could someone help me to analyze this problems please? Thanks sincerely.

The schematic is enclosed for you reference.

  • I don't see anything that jumps out at me on teh schematic.  Can you provide some waveforms?  Specifically, PH and SS/ENA to start with.  You will probably need to trigger on the rising edge of VIN to see what is happening as teh IC attempts to start up.