Hello,
I'm having problems with the TPS6102x parts. I have tried the 20 (adj), 26 (fixed at 5V) and 29 (adj) versions and get the same problems. The parts do work but when I try to modify components to change the output voltage, the part fries itself every time. I have tried some on my board and even on a TPS61020EVM with the same results. I'm trying to take a 3.0-4.2V input and make a 5V output.
The datasheet has some weird suggestions that lead to terrible results. The TPS61020EVM uses R3 = 1M and R4 = 178K which is designed to output 3.3V. The EVM violates the datasheet immediately with R4 being less than 200K and not having a parallel capacitance across R3 (see page 15 of TPS61020 datasheet). Since a 3.3V output isn't what I wanted, I tried to change the values to get the 5V I need (actually around 5.06V to allow a bit extra for line losses in my application). I changed R4 to 110K. The result was that it produced about 4.4V at the output (no load attached) which wasn't right. I thought that maybe I had to have that capacitance to deal with R4 being >200K. The calculated value was around 16pF and I had some 18pF's laying around. The problem is that if you actually do solder in that capacitor it fries the chip and burns up the board as it tries to pull 1.4A from the input supply! On page 17 it talks about another application of the small capacitance across R3 for small signal stability. The EVM has a 100m ohm ceramic capacitor so it isn't needed but this confusion in capacitor usage is not good and the results are disasterous (as I have repeated on several boards over months of testing without knowing why). Maybe there is a typo and the cap belongs across R4 or something? The EVM doesn't use it so maybe they have since learned it is a bad idea and they should tell customers.
In my design, I use R3= 2.2M and R4 = 240K in order to get the 5.06V I require. It works, but if you even so much as touch the part while it is active: POOF! It's dead and the input is short circuited which means it starts pulling all kinds of current and heating up the PCB. My station is grounded so I don't believe this is an ESD issue and it seems like this part is hyper sensitive to capacitance on its feedback pins (created by my finger in the case of touching it).
Based on the basic schematic in the datasheet and TPS61020EVM user manual, how would you design in this chip to make a stable power supply using the input and output parameters listed in the first paragraph? What resistor values do you recommend? Is this chip that sensitive and this is a known issue? The only way I can test chip heating under full load is to touch it carefully and I have never used a chip so non-robust in my life! Are there errors in the datasheet when it comes to this capacitive compensation? I really don't want to put this part in the field in a customer application and have it fry itself for some unknown and unpredictable reason. Please help.
Thanks!
References: http://focus.ti.com/docs/prod/folders/print/tps61020.html http://focus.ti.com/docs/toolsw/folders/print/tps61020evm-025.html