Ryuji Asaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ryuji,
We are in the process of updating the TPS22965 datasheet with the SOA curves you are looking for. In the meantime, could you tell us about your application use case? What is the max ambient temperature of your application? What is the current profile of your application (duty cycle of the load)?
Ryuji-san,
1. tps27081a will break
2. It can do either, depending on how the metal melts. Most likely open though.
3. The curve falls exponentially because, as temp rises VT (threshold voltage) rises. At Vgs=1.2V you are already much closer to the threshold than the other figures. Essentially the part is being turned off, that is why you see the sharp decrease.
The TPS22965 can be used under the conditions you listed without any reliability concerns.