Hi,
Im trying to go from 12V to 15V but I seem to be having an issue. I
have the inverting setup giving me -15V and it works fine, but I cant
get the +15V to work. In this data sheet
http://focus.ti.com/lit/ds/symlink/mc34063a.pdf
on page 6 there is the circuit im using. I dont know about the
value of the resistor connected to pin 8, so I used a 220Ω. My values
that I calculated are listed below.
L=25uH
Diode= Schottkey Vf=0.5V
Rsense=100mΩ R1=1k pot R2=10k
CT=300pF Co=5uF
Any ideas?
Thanks!