Hello,
I am reading the application report:Phase-Shifted Full-Bridge, Zero-Voltage Transition Design Considerations,SLUA107A.
on page 15, the fourth paragraph copied below: it says there is a Practical Applications section .
"If the resonant inductor value is too large it may take too long to reach the necessary load current
within the conversion cycle. The calculated inductor value satisfies the light load condition, however
full load operation must also be evaluated. Details of possible solutions to this are highlighted in the
Practical Applications section of this paper."
However, there is no such section in the paper.
Anybody can help find the section or help explain the meaning of the paragraph?
Thanks a lot,