This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92075 buck-boost

1) Per SLVU813 EVM Figure 5, and also I measured the FET source voltage, the peak goes to 1.2v. According to the datasheet this is the Vcl(current limit). In normal operation, would the ISNS voltage be ~0.5V, and only on an overcurrent/inductor short would the current limit be reached?

2) The device runs in CCM and at the lower voltages/currents in DCM. Can this design be converted to a DCM/BCM mode only?

 

Your feedback is most appreciated...thanks.