This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

regulate 12V down to -55V



Hey guys, I am trying to find a Ti chip that will allow me to regulate a 12VDC input to -55VDC,

I could not find any thing that goes as low as -55VDC,

Since, I am new at power management.

My question is:

Do those kind of chip even exist(TI chip or chip from other company)?

if not  ,Is there any other way to get -55VDC?

  • Hello Zhen,

    Welcome to the Forum!

    With DC power supplies, the simplest way I can think of explaining it is that you can use the same chip, MOSFET, etc, to achieve a negative voltage output.  You can also use diodes and capacitors as well.  If you are familiar with switch mode power supplies and transformers then you will know that a negative component is created on the output side that can be used.  

    It is more a technique than an actual device.  In fact, you can create an adjustable voltage regulator using an opamp and a precision 2.5V regulator.  There are resource available on the TI website for designing power supplies, you can search the site for more information.

    The other point is that a negative voltage can be thought of as a positive voltage supply connected with the ground reference reversed.  If you have a dual output power supply, you can connect the outputs together and generate a full scale positive and full scale negative voltage from the unit.  You can search the web for how to connect up a dual power supply to generate negative voltages.

    Depending on whether you just need something for doing a test or you need to supply these voltages for a stand alone device, will determine which of the above techniques to use.

    Thanks,

  • Hi Zhen,

     

    What output power do you need? That will mainly determine the type of power supply you need.

    Or in Greenja's words: the technique you need.

  • The -55V draws maximum 30mA or 1.65W.  I would consider a efficiency of +65% to be effective.


    The data sheet did not specify the tolerance of this supply.
    It only states:
    "VSUB(-55V) must be the most negative potential of the IC."
    and also the ABSOLUTE MAXIMUM RATINGS says that It can not go beyond −60V.

    As you can see, the power requirement is not big.  I hope i can find a chip that allow me to go down to -55 easily.

    Also , i hope I can avoid the use of transformer, and reply solely on inductor.(but not necessarily)

    .Since i am a first year engineering student,  I do not have the ability to "design the wheel" or implement some high level design.

    So that is why i am simply  looking for a chip to help me get there.

  • I would suggest to just enter these values in the WEBENCH® Designer (http://www.ti.com/lsds/ti/analog/webench/overview.page)
    I entered:
     
    Vin_min = 11V
    Vin_max = 13V
    Vout= -55V
    Iout= 0.03A
     
    which gives several designs.