I'm working on a new design and am trialling a TPS62143. I'm just testing a couple of prototype boards and have come across an unusual problem which is knocking my confidence on this part.
I built up 2 boards and both worked fine. However I was probing around on one with a multimeter and when I finished I noticed the circuit drawing far more current - for about a 6V input it was drawing a current around 200mA for a circuit that only consumes about 5mA (there is another circuit that is plugged in that takes upwards of 1A hance the high current requirement). My first thought was I must have shorted something out with my probing and somehow blown the regulator. However the strange thing was that the 5V O/P from the regulator was still up so the rest of the circuit was happy but the regulator started getting very hot (but ultimately it'll still run like this).
OK, I chalked that up to one of those things and that I must have inadvertedly b*ggered something up. I switched to working with the backup board and for a long while everything was fine. I was making some "designer mods" to the circuit - well away from anything regulator - in a prototyping area and when I powered up, this board now has the exact same problem - which tends to imply a fundamental design issue somewhere in my circuit.
The regulator schematic and BOM are WebBench generated (I can post the schematic when I'm back in the office). Input voltages during these tests was around 6V for a 5V O/P.
I haven't had a chance to scope the 5V line when "failed" but a DMM measure of the output shows no shorts or low resistance. When operating normally the TPS62143 doesn't get hot even with currents 500mA, but with a light load and drawing its 200mA it does.
Anything immediately spring to mind with anyone? The end application has a prototyping area for users to add their own customisations so I need something that is robust.
Any thoughts?