Hi,
I am desinging a 2KW PFC controller with the UC2818 controller. One of the requeriments of this design is that the
input voltage could be compressed between 380VAC to 440VAC, 50Hz. I have already validate my PFC when the voltage
is less, with 220V to 250V, and the results were satisfactory. But when I change the input voltage, and all the resistances and
capacitors as the datasheed suggest, the results are bad, the Power Factor only is 0.9 at low power, and then decreases.
Please help me if you know something.
Thanks!