This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353 Circuit Design

Other Parts Discussed in Thread: TPS53353, TPS53355

I'm having difficulty getting the TI TPS53353 switching regulator working.  I designed the circuit to produce a 5V output from a 15V input.  Here are pictures of the schematic and layout (0804.TPS53353.pdf).  The layout shows the top and bottom layers, there are also an internal ground plane and an internal layer for +5V_Fused (connected to vias on output of fuse F3) that are not shown.  Values of the passive components were calculated using the table below.

When I supplied the 15V the regulator's output was fluctuating when observed on a voltmeter and there was audible clicking coming fromt the chip.  After about 30 sec of being powered, a bit of fire and then smoke came out of the chip and I quickly shut off the 15V supply.

The ceramic caps are all X5R/X7R.  Could the problem be that the capacitor values are too far off?  Should I be using C0G/NP0 caps?


The outout electrolytic caps used have an ESR of 13 mOhm (6.5 mOhm in ||), but the design originally specified using caps with an ESR of 17 mOhm (8.5 mOhm in ||), as listed in the excel file).  Could a too low ESR cause stability issues?

After the chip popped, it was removed and pins 19 (VDD) and 20 (MODE) were seen to be blown off the chip and their pads where blown off the board.  With the board as it is now, pins 19 and 20 are shorted, but that may have happened when the chip blew.  If they were shorted to start with, could that have caused the chip to blow?

Any other thoughts on what might be wrong with my design?

Thank you.

TPS53355 Component Values
Parameter Value Description Datasheet Location Notes
Vin (V) 15 Input voltage
Vout (V) 5
Imax (A) 20 Maximum load current
Iocp (A) 25 Over-current protection threshold
Fsw (Hz) 500000 Switching frequency Table 2 (p.16)
Rrf (Ohms) Open Fsw select resistor Table 2 (p.16)
R2 (Ohms) 10000 Output voltage set resistor 2
Rmode (Ohms) 39000 Mode set resistor Table 1 (p. 15) Connect to ground
Rds (Ohms) 0.0016 Internal switch resistance @ Iocp Step 6 (p. 21)
Itrip (A) 0.00001 Current through Rtrip @ Iocp Step 6 (p. 21)
Ideal Values Formula
Iripple (A) 6.666666667 Inductor ripple current Step 3 (p. 20) Iripple = Imax/3
L (H) 1.00E-06 Inductor value Eq. 6 (p. 20) L = (3/(Imax*Fsw))*((Vin - Vout)*Vout/Vin)
Vtrip (V) 1.109333333 Voltage on Rtrip @ Iocp Eq. 3 (p. 18) Vtrip = 16*Rds*(2*Iocp - Iripple)
Rtrip (Ohms) 110933.3333 Rtrip value Eq. 2 (p. 18) Rtrip = Vtrip/Itrip
Ipk (A) 28.33333333 Peak inductor current Eq. 7 (p. 20) Ipk = Vtrip/(32*Rds) + (1/(L*Fsw))*((Vin - Vout)*Vout/Vin)
ESR (Ohms) 0.008333333 Ouput capacitor ESR Eq. 8 (p. 20) ESR = L*Fsw/60
R1 (Ohms) 72870.37037 Output voltage set resistor 1 Eq. 9 (p. 20) R1 = (Vout - (Iripple*ESR/2) - 0.6)*R2/0.6
Real Values - Calculated using component values
L (H) 9.60E-07 Inductor value Vishay Dale IHLP5050FDER1R0M01
ESR (Ohms) 0.0085 Ouput capacitor ESR (2 in parallel) Nichicon RHT1A331MDN1
Rtrip (Ohms) 110000 Rtrip value
R1 (Ohms) 73200 Output voltage set resistor 1
R2 (Ohms) 10000 Output voltage set resistor 2
Rrf (Ohms) Open Fsw select resistor
Vout (V) 5.020333333 Output voltage Eq. 9 (p. 20) Vout = (R1*0.6/R2) + (Iripple*ESR/2) + 0.6
Vtrip (V) 1.1 Vtrip value Eq. 2 (p. 18) Vtrip = Itrip*Rtrip
Ipk (A) 28.42881944 Peak inductor current