This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI fusion power designer UCD3xxx GUI

Other Parts Discussed in Thread: UCD3138

Hi all,

I am working with UCD3138. I have some code for LLC resonant converter using CCS 3.3, and is working without any error.
But I am not able to load it on the board to see the PWM signals.

Also, I tried to use TI fusion power designer UCD3xxx GUI to do so, but failed. The problem is that my USB interface adaptor is not communicating with my PC. The UCD3138 LED as well as the adaptor LED are on, but not working, and I get the following error.

“Could not connect to remote USB adapter server @:8090 “

Can you please help me to fix this problem.

 

Thanks,

Mehran