This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm5122 : Problem on the SOFT-START Css capacitor evaluation

Other Parts Discussed in Thread: LM5122

hi all
I want to use the lm5122 to convert 12V to 5 V (with high output current 5A to 10 A).
I chose the lm5122 because in the near future this output voltage will be greater ( 48V max).
But my problem today is the SOFT-START which is programed by the Css capacitor. In the data sheet the equation 11 give me a negative time (because my input voltage is bigger than my output voltage) ????
Some one can give me some informations concerning this observation?
how can i estimate tss?
For the end, if the lm5122 can realise my specifications??
Thank all
Penef