Is it possible to charge when the host processor is in an off state?
I am looking at this series of parts because it can look at D+ and D- to detect a dedicated USB charger. This is a required feature for my application.
Is there any way to use an i2c charger when the host processor is completely off? It seems it may work, but will set the USB current limit to 100mA which is too low.
Are there any parts that satisfy these requirements:
- Charge at 900mA if connected to dedicated USB charger, regardless if device is powered on or off
- Charge at 500mA if USB host will allow that much current, regardless if device is powered on or off
Thanks.