Hi,
This is generic question about the cell balancing algorithm for Impedance Track devices, specifically the battery in question uses the bq20z65-R1. I understand that for the cell balancing algorithm to work a Qmax update needs to happen for the fuel gauge to determine the individual capacity differences for each cell group. For the Qmax update to happen there needs to be several several hours of rest time until the slope of the voltage decays to 4uV/s. My question is what happens if the Qmax update happens while there is still charging voltage applied, but yet the current has decayed below the min relaxation value of say 50mA or less? In the end user application it is very unlikely that the battery will ever be in an OCV condition, the battery will either be discharging, charging, or sitting fully charge at some nominal float voltage. In this scenario can the Qmax update be trusted since during the "relaxation" mode the voltage values will largely be inflated? Does IT not work for this type of application?