This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fixed/ High Frequency DCDC converter (no PFM or disable PFM)

Guru 20090 points
Other Parts Discussed in Thread: TPS62110, TPS62140
Hello,
 
I'm serching DCDC converter of below conditions.
I can't find device in this condition... Duty cycle or Eco mode is bottleneck in this conditions.
 
Vin(min)5.5V
Vin(max): 10V
Vout: 4.8V
Iout: 1.5A
Fsw:1MHz ~ 2MHz
No need PFM mode , ECO mode. if we can disable PFM , it is OK.
 
Could you please kindly let me know the device if there is ?
 
Best Regards,
Ryuji Asaka